Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the analog output of the ATV61 or ATV71 be set up as 0-10 VDC instead of 4-20 mA?
Issue:
Needs to set up a analog output of the ATV61 or ATV71 drive, to be set up as 0-10 VDC instead of 4-20 mA.

Product Line:
ATV61 and ATV71

Environment:
All

Cause:
NA

Resolution:
Yes.
Go to the Input/Output menu (1.5) and set AO1 type to voltage (0-10v range). Set AO1 assignment to the proper setting. The minimum and maxim range can also be adjusted inside the 0-10 V or 4-20  mA ranges.