Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the ATV61 or ATV71 have the COS (cosine, power factor) parameter?

Article available in these languages: Spanish

Issue:
The ATV61 or ATV71 COS (cosine, power factor) parameter.

Product Line:
Altivar 61/71

Environment:
All

Cause:
Application inquiry: What horsepower range of 3 phase motors can be controlled by a ATV58 single phase 208/230vac input Drive?

Resolution:
No, there is no power factor setting in these drives.

Set motor parameters in menu 1.4 (Motor Control - drc)
Run auto tuning, and make sure the motor is cold before doing the auto tuning function.