Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Is it possible to install the Fusarc fuse in the upstream of LBS (Load Break Switch).

Yes, it is possible to install the Fusarc fuses in the upstream of Load Break Switch (LBS) switch.

Note:
1. Refer the attached sheet to choose and install the right fuse.
2. The current rating for the Fusarc Fuses has also been provided in the attached document.

Schneider Electric Egypt and North East Africa

Attachment(s)
Fusarc Selection.pdf [192.17 KB]