Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Which power phases are controlled by Altistart 01 Soft-Starter?

Article available in these languages: Finnish

The power phases that are controlled by Altistart 01 Soft-Starter are as follows:

In N1 Range of Altistart 01 Soft-Starter only 1 Phase is controlled and that is L1, L2 and L3 are uncontrolled.
In N2 Range of Altistart 01 Soft-Starter only 2 Phases are controlled and that is L2 and L3, L1 is uncontrolled.