Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the difference between Fire Mode (Function 52) and Force Mode (Function 53) in Altivar 21 Drive.

Article available in these languages: Finnish, French, Dutch

The difference between the Fire Mode (Function 52) and Force Mode (Function 53) is as follows:

In Fire Mode (Function 52) the Drive will run until it fails, any Fault and/or Stop command will not work. In this function the drive cannot be stopped unless power is removed.
In the Force Mode (Function 53) the Drive runs but critical fault and/or Keypad Stop will stop the drive.
The Critical faults are:
Over Current (OC), Overvoltage (OP), motor current sensor error (Err7), Under Voltage (UP1), Ground Fault (EF2), OCP and excessive torque boost fault (E-20).
Refer attachment for the list of faults.

Schneider Electric Egypt and North East Africa

Attachment(s)
Altivar 21 Critical Fault List.pdf [42.12 KB]