Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between LAD703 and LA7D03
Issue:
Identifying differences between two similar part numbers

Product Line:
IEC contactors and starters

Environment:
Products sold and used in the United States

Cause:
Identifying differences between two similar part numbers

Resolution:
Both will remotely stop (trip) or electrically reset the overload, however;
LAD703 is used on Tesys overload LRD01 through LRD35 and LR3D01 to LR3D35.
LA7D03 is used on all other LR*D overload relays other than LRD01 to LRD35 and LR3D01 to LR3D35.*

*LR9D01-LR9D32 electronic overload relays do not currently have a remote reset module accessory

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center