Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the protective covers for power terminals on the ATS48 softstarters?
Issue :
ATS48 protective covers for power terminals

Product Line :
Altistart Soft start

Environment :
ATS48

Cause :
Finger protection

Resolution :
Covers are only available for the larger frame sizes of the Altistart 48.

LA9F702 - cover for ATS48C14Y and ATS48C17Y
LA9F703 - cover for ATS48C21Y, ATS48C25Y, ATS48C32Y

*Each part number has a set of 6 terminal covers.

Schneider Electric Egypt and North East Africa