Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for ATV61 and ATV71 Ethernet IP card?
Issue:
ATV61 and ATV71 Ethernet IP card part number

Product Line:
Altivar 61 and Altivar 71 drives, all serial numbers

Environment:
All

Cause:
Need part number for Ethernet IP card

Resolution:
The part number for the Ethernet IP card is VW3A3316. This card has Ethernet IP functionality only.
The VW3A3320 option card has Ethernet IP and Modbus TCP functionality.