Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do QED switchboards come with any Lifting Brackets/ Spanner Bars, Straps, Riggings, or Rollers?
Issue:
QED switchboards includes Lifting Brackets / Spanner Bars, Lifting straps, or Rollers

Product Line:
QED SWBD

Environment:
Installation

Cause:
Rigging

Resolution:
Schneider Electric provides lifting straps as standard equipment for NEMA Type 1 switchboard shipping sections rated 3,000 A or less.
Lifting straps are NOT furnished on shipping sections rated more than 3,000 A, or on Outdoor (Nema 3R) switchboards.
Spanner bars , brackets, riggings , or rollers are not furnished  for any SWBD's shipped and are provided by end user.


Detailed information can be found in Instruction Bulletin 80043-055-12, Power-Style QED-2 Switchboards. This bulletin is attached for reference.

Schneider Electric Egypt and North East Africa

Attachment(s)
80043-055-12.pdf [5.68 MB]