How can we help you today?

Are alternative lugs available for an HVMB305200 Minibreak Medium voltage switch?

Issue:
Alternative lugs available for an HVMB305200 minibreak switch

Product Line:
HVL Mini break

Environment:
Installation

Cause:
Alternate wire size

Resolution:
No. There are no alternative lugs available for the compact Mini break switches.
This is due to the lack of wire bending space available with the need to accomodate larger wire or more conductors.

Set screw cable lugs for #14 solid—2/0 stranded aluminum or copper cable are provided for two line and one load connections

Schneider Electric Egypt and North East Africa
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
  • Help and Contact Center