Issue:
Is a TVSS unit catalog number TVS4EMA16A compliant with specification UL1449 3rd edition?
Product Line:
TVSS.
Environment:
Products sold in the United States.
Cause:
Product features.
Resolution:
Yes, a TVSS unit TVS4EMA16A has a UL1449 3rd edition listing, and has an identification sticker on the inside of the unit that indicates this.
NOTE: The TVS4EMA16A is obsolete and replaced by the SSP04EMA16 (in a NEMA 1 enclosure or SSP04EMA16S in a NEMA 4 SS enclosure) and the SSP04EMA16 is UL1449 5th edition listed.
CTA-ID : 2053576
Is a TVSS unit catalog number TVS4EMA16A compliant with specification UL1449 3rd edition?
Product Line:
TVSS.
Environment:
Products sold in the United States.
Cause:
Product features.
Resolution:
Yes, a TVSS unit TVS4EMA16A has a UL1449 3rd edition listing, and has an identification sticker on the inside of the unit that indicates this.
NOTE: The TVS4EMA16A is obsolete and replaced by the SSP04EMA16 (in a NEMA 1 enclosure or SSP04EMA16S in a NEMA 4 SS enclosure) and the SSP04EMA16 is UL1449 5th edition listed.
CTA-ID : 2053576
Released for: Schneider Electric Egypt and North East Africa