Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Soft Starter ATS48 is displaying nLP fault ?
nLP means No Line Power
Cause :This fault appears when powering up the control part without powering up the power part .
Remedy : Connect power to terminals: 1/L1,3/L2,5/L3