Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
For the LC1D Contactors (Tesys "D" range), what is the difference between utilization categories AC-1 and AC-3?

For the Tesys "D" Range of contactors,
- AC-1 Utilization category: it is a general category that describes the resistive, non-inductive or slightly inductive loads (mainly power factor of load 0.95 or more) and it cannot be used to describe AC motors.
- AC-3 Utilization Category: it is a general category describes all Squirrel cage motors during starting, breaking or motor running.

The Tesys "D" contactors can be used with both categories according to the application and the nature of load.

(note: the same contactor used for both categories with de-rating - there is no specific contactor reference per category).