This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Remote display terminal for ATV31 is ( VW3A31101 ). It doesn't contain a jog dial like the graphic display terminal used with ATV312, but the speed can be varried using the menu, or by using an external potentiometer for the drive. It has all the other functions of the graphic display ( VW3A1101 ).
Find attached the datasheet and the installation manual for ( VW3A31101 ).
Find attached the datasheet and the installation manual for ( VW3A31101 ).
Released for: Schneider Electric Egypt and North East Africa