Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to adjust the settings of soft starter ATS48 to operate multiple motors in a cascading way ?
In order to activate the cascading function of the soft starter you need to do the following :
Set : CSC " Activation of the cascade function " in the drC menu to : On
Set : LI3 " Logic Input " in the I/O menu to : LIC
Set : R1"Relay 1 " in the I/O menu to : r1I

Schneider Electric Egypt and North East Africa