Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How can I know the status of the primary & secondary controller? Which is primary & which is secondary & which is in offline mode , For Quantum Hotstandby ?
There is a system word %SW61, it is a readable register & is used to monitor the current machine status of the Primary & Standby.

This word consists of 16 bits, According to their status (0 or 1), we can determine the following:

1- First PLC is offline, primary or secondary
2- Second PLC is offline, primary or secondary
3- PLCs having matching logic or not
4- Hot standby is active or not

Schneider Electric Egypt and North East Africa

Attachment(s)
SW61.pdf [34.22 KB]