How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

I have a TSX Micro module, the " Ter " & the " Run " Leds are blinking and the I/O led is off ?

This means that the PLC is in the STOP mode. It has to be run using the program ( Connect the module to the PC ).

Schneider Electric Egypt and North East Africa
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
  • Help and Contact Center