Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
While downloading a Program from Vijeo designer lite to XBTR terminal , It displays No Terminal connected ?
To be able to connect and download the program using TSXCUSB485+XBTZ925, you need to install the Uni-Telway driver version 1.8 or later
These drivers are available :
-On terminal Coniguration software CD-ROM
-To order (reference TLX-CDDRV20M)
Below are the reasons why the software may display the message " No terminal connected " :
- The XBT-Z925 cable is not connected correctly.
- The TSX-CUSB485 cable is not connected to the USB port.
- The driver is not configured correctly.
- The TSX-CUSB485 cable driver is not installed.
- The selector switch on the TSX-CUSB485 cable is set to 2 or 3. Transfer is only possible if the selector switch is in position 0 or 1.
- Turn the XBT-Z925(A) cable round as this cable has two cable ends that are not symmetrical.

The attached instruction sheet clarifies the correct configuration for the driver

Schneider Electric Egypt and North East Africa

Attachment(s)
Instruction sheet XBTZ925 adapter.pdf [513.75 KB]