Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the Main Function of MN Coil in MCCB NSX and how it is operated ?
The MCCB of type NSX (all ratings till 630 A) can be supplied with MN release coil

its main function is under voltage protection to the MCCB (it protects the CB from undervoltage case that could happen to the supply of the MCCB)

The MN (under voltage release coil) operates if the supply input voltage to the MCCB decreased till it reach 0.7 Un and trip the CB

It doesn't close the CB again until the Supply voltage increase above 0.85 Un (to make sure that the under voltage situation is finished)