This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Vijeo Designer V5.0 is not compatible with the windows 7 (64bit), It is compatible with the below operating systems:
-Windows XP Professional (32-bit)
-Windows Vista (32-bit)
-Windows 7 (32-bit)
Vijeo designer V6.1 is compatible with windows 7 Business Professional (32 or 64 bits )
-Windows XP Professional (32-bit)
-Windows Vista (32-bit)
-Windows 7 (32-bit)
Vijeo designer V6.1 is compatible with windows 7 Business Professional (32 or 64 bits )
Released for:Schneider Electric Egypt and North East Africa