{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PowerChute Network Shutdown 2.2.4 and 4.5G and 5G Smart UPS Behavior

Issue

When using Powerchute Network Shutdown 2.2.4 and Network Management Card 2 UPS application firmware revision apc_hw05_sumx_v5.0.3 (SFSUMX503), selecting the option to turn off the UPS via PowerChute Network Shutdown is supported for only the 'On Battery' and 'Low Battery' UPS events on certain Smart-UPS models.

Should a user attempt to use the turn off UPS functionality via PowerChute Network Shutdown for other events, the UPS will not turn off. Furthermore, should the user restart the server running PowerChute Network Shutdown, the server will shutdown immediately.



Product Line

  • Smart-UPS Models:
    • SMT750
    • SMT1000
    • SMT1500
    • SMT2200
    • SMT3000
    • SMX750
    • SMX1000
    • SMX1500RM2U
    • SMX1500RM2UNC
    • SMX2000RMLV2U
    • SMX2200RMLV2U
    • SMX3000RMLV2U
    • SMX3000RMLV2UNC
  • UPS Network Management Card 2
    • AP9630
    • AP9631



Environment

  • AP9630/31 sumx application v5.0.3
  • All serial numbers


Cause

This is due to the initial implementation of v5.0.3 sumx application for particular UPS models.



Resolution

It is recommended that users upgrade to SUMX application 5.1.1 or higher to resolve this issue at http://www.apc.com/tools/download.

In order to rectify the server restart/shutdown situation without upgrading, the user must manually turn off the UPS and then turn it back on.




Please note: Any prior version of PowerChute Network Shutdown will not work with the aforementioned UPS models.



Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.