{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you hardwire the input/output of the Matrix-UPS?
Issue:
Can the input or output of a Matrix UPS be hardwired?

Product Line:
Matrix UPS

Environment:
All serial ranges

Cause:
A user may wish to hardwire the input/output of the UPS rather than use the supplied input power cord.

Resolution:
APC offers a hardwire kit to be used with the 120/208 Matrix-UPS product. The part #s for these kits are as follows:

MXA001: 5kVA Hardwire kit
MXA002: 3kVA Hardwire kit

These hardwire kits replace the standard back plate and allows the input and output of the Matrix to be wired directly to their corresponding electrical panels. This kit provides 120V, 208V and 240V on the output. The electrical specifications for both the Matrix 3kVA and Matrix 5kVA UPS systems are as follows:

Input Over-current Protection
3kVA: 20 A
5kVA: 30 A

Input/Output Wire Size
3kVA: 12 AWG
5kVA: 10 AWG


Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.