Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Description of NEMA L6-30 Receptacle

The NEMA L6-30 is used for input on the domestic APC Matrix-UPS, Smart-UPS T models, and Symmetra RM 2-6kva UPS.  The NEMA L6-30 receptacle is also used as an output receptacle for supplying 208 VAC in the Matrix-UPS, the Smart-UPS T models, and single phase Symmetra systems (Power Array, RM, LX).  It is a locking two-pole, three-wire grounding receptacle with a maximum input of 250V and 30A. When used with APC's UPS models, the receptacle will generally provide either 208V or 240V(depending on the UPS model). This receptacle requires that three connections be made (see diagram below).

G= Ground
X= L1 (Hot)
Y= L2 (Hot)


img11


As previously mentioned, this is a locking receptacle. After insertion, turn the plug clockwise to lock.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center