Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Is the Vijeo Citect drivers support ModbusPlus communication with PCI-85 communication card, If yes, does it need any special software package or not (such as MBX software with version > V.4?
Vijeo Citect Support Modbus Plus Communication with PCI-85 Communuication card.
Vijeo Citect MBPLUS Driver supports communication with Modicon PLCs via an SA85 or PCI-85 interface card.
Communication is through the Modbus plus port on the PLC. You can connect Vijeo Citect to multiple Modicon PLCs using a modbus plus network

1) MBX driver Version > 4.0 dose not support the operating system windows 7 or Windows server 2008.
2) For Modbus Plus Communication you need MBX Driver software V7.1 or higher.
3) The PCI card 416NHM30032 only works on a +5v bus.kindly check your machine PCI slot specification.
4) Vijeo Citect 7.2 Vijeo Citect MBPLUS Driver supports communication with Modicon PLCs via an SA85 or PCI-85 interface card.
5) 416NHM30032 & MBX4.0 Both are obsolete product. There is no longer any engineering support as this product was made obsolete

Schneider Electric Egypt and North East Africa

Attachment(s)
Using SA85 Modbus Plus Card.pdf [253.06 KB]