This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
.compact NSX circuit breakers may be used between -25°C and +70°C. For temperatures higher than 40°C(65°C circuit breakers used to protect motor feeders), devices must be derated
.Circuit breaker should be put into service under normal ambient, operating-temperature condition. Exceptionally, the circuit breaker may be put into service when the ambient temperature is between -35°C and -25°C
.The permissible storage-temperature range for compact NSX circuit breakers in the original packing is -50°C and +85°C
Released for: Schneider Electric Egypt and North East Africa