This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
IP standards are user to describe the degree of protection of objects against solid bodies and liquids. The first number describes the protection against solid bodies, while the second number is for the protection against liquids.
As for IK standards, they're used to describe the protection of objects against mechanical impacts.
As for IK standards, they're used to describe the protection of objects against mechanical impacts.
Released for: Schneider Electric Egypt and North East Africa