Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the cooling fan for the ATV71HD18N4?
Issue:
Looking for the part number for the cooling fan for the ATV71HD18N4?


Product Line:
ATV71

Environment:
Cooling Fan

Cause:
n/a

Resolution:
VZ3V1205 is the heatsink fan kit.  The fan measures 3.14 inches by 1.5 inches.  This drive uses one fan kit per drive.