Issue:
Customer needs to find computer comm ports for firmware update.
Product line:
Computer
Environment:
Windows XP
Cause:
Install/Repair
Resolution
WINDOWS XP Display Interface
- Click the START in the lower left corner
- Go to Settings
- Click on Control Panel
- Open the System folder
- Click Hardware in the tabs then click the Device Manager toward the middle
- Click the [+] next to Ports and look for USB to Serial Cable
Note: Another way is to find My Computer on your desktop and right click. Open Manage and look for Device Manager on the left side then Device Manager. See picture below.
Released for: Schneider Electric Egypt and North East Africa