Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What are the protection functions available in ATS48 ?

1. Machine and motor protection functions :
1.1. Built-in motor thermal protection.
1.2. Processing of information from PTC thermal probes.
1.3. Monitoring of the starting time.
1.4. Motor preheating function.
1.5. Protection against under loads and over currents during continuous operation.

2. Line Protection:
2.1. Phase failure is indicated by output relay.