Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the command word for the ATS22 soft starters for network communication?

Issue:
Command word for the ATS22 soft starters.

Product Line:
Altistart ATS22

Environment:
All

Cause:
Modbus address for ATS22

Resolution:
The command word address for the ATS22 soft starter is 752.
The ETA status word address for the ATS22 soft starter is 256

See the attached PDF document for the Command word and the ETA status bit assignments.

Schneider Electric Egypt and North East Africa

Attachment(s)
Modbus address words for the ATS22.pdf [332.67 KB]