Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can you change the display screen to show different parameters on the ATV61 and ATV71 drives?
Issue:
How can you change the monitoring screen to show different parameters other then frequency reference on the ATV61 and ATV71 drives?

Product Line:
ATV61, ATV71.

Environment:
All model numbers, all serial numbers.

Cause:
Customer wanted to monitor output frequency and output current on the monitor screen.

Resolution:

Under Main Menu,
Go into Menu 6 Monitoring Configuration.
6.2 Monitor Screen Type to adjust the number of parameters that can be displayed and the format of display.
There are 3 options; Digital, Bar graph, and List.
Digital and Bar Graph can display up to two parameters at a time on the screen.
List displays up to 5 different parameters on the screen.

Go into Menu 6.2 Parameter Selection to select the parameters that are desired.  Parameters can also be removed by removing the check mark in the box.
When you are done hit ESC to back out until you see your new display parameters.