Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is a line reactor required with the ATV61 or ATV71 drives if the DC choke is not used?
Issue:
ATV61/ATV71 Line reactor or DC choke requirements

Product Line:
Altivar 61 71 ATV61 ATV71

Environment:
High HP units, greater than 100HP, 460V, greater than 75HP, 230V

Cause:
DC chokes are included standard, but the drives can be ordered without a DC choke - form D.

Resolution:
If the DC choke is not used, a 5% line reactor must be installed on the line side of the drive.
This applies to ATV61/71 sizes:
125 HP 460V and above
75 HP 230V  and above

Schneider Electric Egypt and North East Africa