Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Are there a 4-Pole thermal overload relays to be used with "D" Contactors - 4 Poles ?
-The "D" type thermal overload relay (LRD) is used for protection of 3-Phase induction motors against over load and as it is a fact that there is no any induction motor of 4 Poles or 3 Poles + Neutral ,so the thermal overload relays are only found in 3 Poles.
- The 4 Pole "D" type contactors are not used with motors. These are used for utilization category AC-1