Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What causes a OP3 fault on the ATV212 drive?

Issue:
OP3 fault on the ATV212 drive

Product Line:
ATV21 ATV212 Altivar 212, Altivar 21 drives

Environment:
All models, All serial numbers

Cause:
OP3 fault is caused by overvoltage during constant speed operation.  This could be caused by abnormal fluctuation of the input voltage, Power networks greater than 200kVA, Power factor correction switching, SCR's switching on the Power network, the load regenerating into the drive or intermittent output phase loss.

Resolution:
Confirm the motor nameplate information matches settings in the drive.  Confirm that the drive is sized correctly for the load and application.

tYP = 2 (60Hz)
tHr = motor FLA
uLu = motor voltage
F415 = motor FLA
F417 = motor RPM

Set F626 = 150% (increases the DC bus overvoltage threshold)
Set AU1 = 0 (disables Auto ramp)

Check the setting of Pt parameter (type of control) matches the application.

Check to make sure that the load is not spinning without drive's input (such as fan applications). If the load is spinning too fast in the wrong direction, the drive won't be able to catch it. If this is the case, try installing a mechanical brake to prevent this issue.

Check the setting of F301 Catch on the fly and try setting it to 4 (Each start)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.