Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How can I upload a program from Xenta 280/300/401 controllers ?

When the application file is generated and compiled, it no longer contains any information about the layout or the "yellow boxes".
Therefore, it is not possible to extract a Menta file (.MTA) from the device. However it is possible to upload the compiled information and download it to another device. This way, it is possible to replace a faulty device even if you no longer have the original application
The procedures are illustrated as follows:

  • Always make sure that you have backup of your application files, as it is not possible to upload the graphical information from the device.
  • To upload the complied application information, you have to start TAC Menta and connect to the actual device via a serial cable.
  1. In TAC Menta, select Options, and Simulate to go to simulate mode.
  2. Select Online.
  3. Select Upload.
  4. Select path and filename. The extension will be *.COD (compiled application file)
  5. Select Save, and the complied application file will be uploaded.

It is not possible to open the *.COD file in edit mode in TAC Menta, you will always have to go to simulate mode before you can open up a stored *.COD file.

To change TAC Menta from Tabular mode to normal mode, just press F5. This requires that you have to open up an existing application file (*.MTA) or select to make a new application.