Issue:
ATV212 or ATV21 set up to start/stop on terminal and ramp to 60 Hz
Product Line:
ATV21, ATV212
Environment:
All models and serial numbers.
Cause:
None
Resolution:
Begin by wiring the remote start switch or relay for two wire control between terminals P24 and F.
Program the nameplate motor parameters into the following parameters:
CODE - DESCRIPTION |
thr - Motor thermal prot. |
uLu - Motor rated voltage |
F415 - Motor rated current |
F417 - Motor rated speed |
Make the following parameter settings:
CODE - DESCRIPTION | SETTING |
LL - Low limit frequency | as desired |
UL - Upper limit freq | 60 |
Dec - Deceleration ramp time | as desired |
ACC - Acceleration ramp time | as desired |
CMOD - Command mode selection | 0 |
“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Released for:Schneider Electric Egypt and North East Africa