Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the maximum breaking capacity for the ACB of type NW - 6300 A ?
The ACB of type NW with rating 6300 A has two breaking capacities:
1- 100 KA
2- 150 KA (Maximum breaking capacity)