Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to get the controller error log from a continuum controller ?

The controller error logs contain useful diagnostic information when it is necessary to troubleshoot a controller or system problem. A lot of what is logged are normal system operations that may assist an engineer in diagnosing a problem in the field.

To get the error logs from various controllers follow the procedures below:

NetControllers - 99xx

  • Dumb terminal in using HyperTerminal
  • Sign into the NetController
  • Press V then E and press Enter over the NetController you are attached to
  • Press F2
  • Hit Alt + Print screen and paste into a Word doc
  • Arrow down to single space or Ctrl+D to page down
  • Hit Alt + Print screen and paste into a Word doc
  • Repeat this process until you are at the end of the errors (up to 200)
  • F4 Exits the error log
  • See the CX Controllers Programmer’s Guide for all terminal keystrokes
  • Email the file to Product Support Services

BCX/i2/B3 Controllers

CX9680/ACX5720/ACX5740/9702 Controllers

Note: You can not retrieve errors from NetController I (CX9900) using this tool

  • Controller Error Log Tool
  • Navigate to C:\Program Files\Continuum
  • Double click on ControllerErrorLogTool.exe to open (This will do an install the first time)
  • Note: The ErrorLogTool.exe is an older version of this utility and will work, but gives less information and does not contain the error lookup feature.
  • Enter in the BCX or master CX IP
  • Transport type = UDP or TCP depending on controller configuration
  • CX Enode ID = AccNetId from the main CX editor
  • Select Continuum in the Mode area, top right

If the controller is a field device then enter the following:

  • CX infinet port = Select the one you want to report on
  • Infinet Node ID = port number of the i2 device you want the error log out of

Once all the above required entries have been made:

  • Click Get Log and the page will populate with any errors
  • Once this runs, select SaveAs and name the file