Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What are the programming languages supported by Vijeo Designer?

There are default languages for the Vijeo designer software like English, French, German, Italian, Spanish & Chinese.


For other languages, there is an option in the software which is to import a language file but this will require the HMI to be reprogrammed from the beginning & also this is not the default language



Here is the below link
https://www.se.com/download/ww/en/details/22880565-Vijeo-designer-V61--IDS-V61/?reference=VJDSNDTGSV61M