Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Is the SCADA Vijeo Citect comply to the IEC standard IEC618501 ?
IEC61850 is the protocol and IEC61850-1 is classified as one of the standards  for this protocol.

We do not have IEC 61850 driver available but as a solution we can integrate device as below :-

1) Use third party gateway IEC 61850 to modbus TCPIP /Modbus serial or any other hardware gateway for which protocol is supported in Vijeo Citect.
2) Else use OPCserver.

Schneider Electric Egypt and North East Africa