Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does the BRF fault mean on the ATV71 drives?

Article available in these languages: Turkish

Issue:
ATV71 drive is getting brake feedback fault (BRF)

Environment:
All models, all serial numbers

Cause:
The brake feedback contact does not match the brake logic control.

Resolution:
This is a brake feedback fault. Check the brake logic control circuit and the feedback circuit.
This function is available under 1.7 Brake logic control submenu.
If BRH b2 is set to 0 the reference is enabled at the end of the brake release time.  If BRH b2 is set to 1 then the reference is enabled when the feedback from brake contact enables a logic input and at the end of the brake release time.
- check the feedback circuit and brake logic control.
- check the mechanical state of the brake.