Issue:
Programming Freewheel Stop on Altivar 61 & 71 Drives
Product line:
ATV61, ATV71
Environment:
All models, all serial numbers
Cause:
Need to change the stop type to support application.
Resolution:

Programming Freewheel Stop on Altivar 61 & 71 Drives
Product line:
ATV61, ATV71
Environment:
All models, all serial numbers
Cause:
Need to change the stop type to support application.
Resolution:
- Go into the Application menu 1.7
- Enter Stop configuration
- Enter " type of stop"
- Change SST (type of stop) value to NST and enter.
Released for:Schneider Electric Egypt and North East Africa