Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the size of the DC choke used with an ATV61HC25N4 and ATV61HC40N4?

Issue:
DC choke dimensional size used with an ATV61HC25N4 and ATV61HC40N4.

Product line:
Altivar ATV61


Resolution:
The DC choke used with these models is designated DC-CHOKE 3.
There are 2 units per ATV61HC25N4.
There are 3 units per ATV61HC40N4.
See the attached file for dimensional information.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Egypt and North East Africa

Attachment(s)
DC-CHOKE 3.pdf [20.82 KB]