Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How can i update the M340 firmware?

First you need to download the required firmware version then do the below steps attached in the document
https://www.se.com/ww/library/SCHNEIDER_ELECTRIC/SE_LOCAL/APS/203659_0286/M340_upgrade_procedure.pdf

please check the below video :
https://www.youtube.com/watch?v=4ctaPNPtcKU

Here are the steps in brief
- Double click on the “patcher.bat” file
- In a command prompt window, the following text is displayed: NOE IP address?
- Type the IP address of the NOE:  e.g. 138.157.9.53 and then Enter
- Then appears the following message: Connecting to 138.157.9.53…
- If connection is possible then it displays the following message (checking if the NOE needs to be patched):  Checking...
- If the patch is not needed then it displays the following message and finishes the process:
Patch not needed!
- Otherwise it displays the following message and finishes the process by patching the NOE:
Patch is done!

Important notes

• After the Patch is done and before resetting the NOE, launch the UnityLoader and connect it to the NOE: the NOE can be upgraded.

• The Patch is only a temporary one (RAM): if you reset the module before upgrading it, the Patch is lost, and the module gets back to initial state before patching.

• Do not power off during the Patch and before upgrading it.

Schneider Electric Egypt and North East Africa

Attachment(s)
Modicon M340 Firmware - Update procedure.pdf [1.19 MB]