Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the difference between Micrologic 2 and 5 in terms of protection settings possibilities?
  • Micrologic 2 is for basic protection (over load thermal protection & short circuit)
  • Micrologic 5 is also for basic protection (over load & short circuit ) + Zone selectivity so it can discriminate the fault and trip the suitable Circuit breaker to maintain the maximum reliability of the system