Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number of the Main Control board for ATV71HD22N4?
Issue:
ATV71HD22N4:  Need to replace the Main Control board.

Product Line:
ATV71

Environment:
ATV71HO75N4, ATV71HU15N4, ATV71HU22N4, ATV71HU30N4, ATV71HU40N4, ATV71HU55N4, ATV71HU75N4, ATV71HD11N4, ATV71HD15N4, ATV71HD18N4, ATV71HD22N4, ATV71HD30N4, ATV71HD37N4, ATV71HD45N4, ATV71HD55N4, ATV71HD75N4

Cause:
Need the Main Control board part number.

Resolution:
The Main Control board part number for these drive is VX4A71100Y