{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How is a 4-20mA speed reference signal set up on an ATV71/ATV61?

Article available in these languages: Spanish

Issue:
Setting up a 4-20mA signal to an ATV71/ATV61 drive.

Product Line:
ATV61 and ATV71

Environment:
All serial numbers for ATV61 and ATV71

Cause:
Using a 4-20mA signal for speed reference

Resolution:
Wire the 4-20mA analog input to AI2 and COM

Go to menu 1.5 INPUTS/OUTPUTS CFG, submenu AI2 Configuration
Set AI2 Type to Current
Set AI2 Min Value to 4mA and Max Value to 20mA

Go to Menu 1.6 COMMAND
Set  Ref 1 Channel or Ref 2 Channel  to AI2 (if using Ref 2 channel you'll need a logic input assigned to Reference Switching)
Or in Menu 1.7 Application Funct and configure Reference 1B switching and 1B channel (This is set by default in the ATV61,  If using Ref 2 channel, you must set Ref 1b Channel to NO)

Schneider Electric Egypt and North East Africa