{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
AP9613 Dry Contact I/O SmartSlot Card Low Battery Event Indication Not Working


Issue

No matter what the low battery signaling time/low battery duration value is set to on my UPS, the AP9613 Dry Contact I/O SmartSlot card does not activate the "Low Battery" output relay until two minutes of runtime is remaining.



Product Line
  • UPS Device Management
    • AP9613 Dry Contact I/O SmartSlot Card


Environment
  • AP9613 firmware v101
  • Micro-link UPS models including those with the following model prefixes
    • SMT
    • SMX
    • SURTD

Cause

Due to a firmware bug affecting Micro-link UPS types only, the AP9613 always assumes 2 minutes is the low battery signaling time/low battery duration setting no matter what the user sets the value to on the UPS itself.

This does not affect UPS-Link UPS types.


Resolution

This has been addressed with firmware revision v2.0.1.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.