Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What does FIXED DIFFERENTIAL of pressure switch mean ?

Fixed Differential Pressure Switch means: to control/monitor one set point of a Fluid or that the Sensor can only Detect a Single Threshold Point, the Differential range between PH-PB is Fixed.