Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What's the difference between a variable frequency drive (VFD) and a variable speed drive (VSD)?

Article available in these languages: Japanese

  • A Variable Frequency Drive (VFD): is a drive that works on changing the frequency of an AC motor, it always refers and can be used with AC drives only.
  • A Variable Speed Drive (VSD): is a drive that works on changing the speed of a motor by varying the voltage supplied to it regardless of its type, it always refers to either AC Drives or DC Drives.